Unit Enable Determination ASC - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module is responsible for generating a Unit Enable command. This command is generated from a logical combination of a Network and Hardware Mode and the parameters for controlling the restart after a power failure. This module is implemented as a standard Control Activity.

Figure 1. Unit Enable Determination ASC Module

Figure 2. Unit Enable Determination ASC Module Use in Application

Figure 3. Unit Enable Determination ASC Module Activity