The following tables list the controllers and points that you can manually map into an N2 supervisor.
Note: The maximum limits of a General Purpose, Advanced Application, and VAV Controller are different from the maximum limits of N2 devices. Consider these limitations in addition to the guidelines in the following tables.
Network Point Type | Network Point Address | Command Allowed | Can Map to NAE Objects |
---|---|---|---|
AI | 1–8 | Yes | AI, AO, MSI, MSO |
AO | 1–8 | Yes | AI, MSO |
BI | 1–8 | Yes | BI, BO
BI 7–8 can be mapped to Accumulator |
BO | 1–10 | Yes | BO |
ADF | 1–64 | No | AI, MSI |
65–256 | Yes | AI, AO, MSI, MSO | |
ADI | 1–64 | No | AI, MSI |
65–256 | Yes | AI, AO, MSI, MSO | |
BD | 1–64 | No | AI, BI, MSI |
65–256 1 | Yes | AI, AO, BI, BO, MSI, MSO |
Network Point Type | Network Point Address | Command Allowed | Can Map to NAE Objects |
---|---|---|---|
AI | 1–40 | Yes | AI, AO, MSI, MSO |
AO | 1–8 | Yes | AO |
BI | 1–37 | Yes | BI, BO
BI 4 can be mapped to computer |
BO | 1–14 | Yes | BO |
ADF | 1–64 | No | AI, MSI |
65–256 | Yes | AI, AO, MSI, MSO | |
ADI | 1–64 | No | AI, MSI |
65–256 | Yes | AI, AO, MSI, MSO | |
BD | 1–64 | No | AI, BI, MSI |
65–256 2 | Yes | AI, AO, BI, BO, MSI, MSO |
Network Point Type | Network Point Address | Command Allowed | Can Map to NAE Objects |
---|---|---|---|
AI | 1–6 | Yes | AI, AO, MSI, MSO |
AO | 1–8 | Yes | AI, MSO |
BI | 1–5 | Yes | BI, BO
BI 4 can be mapped to computer |
BO | 1–8 | Yes | BO |
ADF | 1–64 | No | AI, MSI |
65–256 | Yes | AI, AO, MSI, MSO | |
ADI | 1–64 | No | AI, MSI |
65–256 | Yes | AI, AO, MSI, MSO | |
BD | 1–64 | No | AI, BI, MSI |
65–256 3 | Yes | AI, AO, BI, BO, MSI, MSO |
1 BD point addresses 245–248 are reserved for user-defined data storage points.
2 BD point addresses 245–248 are reserved for user-defined data storage points.
3 BD point addresses 245–248 are reserved for user-defined data storage points.