The N2 Mapping tab includes a Device Type setting. The following table shows the appropriate Device Type selection and corresponding controllers.
Device Type Selection | Applicable Controllers |
---|---|
AHU | Generation 1 Application Specific (AS-AHU) |
UNT | Generation 1 Application Specific (AS-UNT) |
VAV | Generation 1 Application Specific (AS-VAV) |
VND | VMA1400, DX9100
All Other Controllers: DC9100, DCM, DR9100, LCP, MIG, NDM, PHX, TC9100, XT9100, XTM, XM1 (XBN), XM2 (XRM), XM3 (XRL or XRE), XM4 (XRL 2x2), XM5 (XRL 2x3), XM^ (XRM 2x2), XM7 (XRM 2x3) |