Module Use in Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This section indicates how the module is identified in the tool software. This section includes a table that lists the individual module instances used by that particular group of modules and the applications in which the module instance is used.

To see a module's connections and how modules interact with it, view the Connections table.