Container Block - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Container folder in the control block palette contains the Activity and Hybrid Activity blocks that act as containers for other blocks. This category also includes a Text block you can use to annotate an application.

Table 1. Container Blocks

Type

Description

Activity

Contains additional logic than what is displayed in the current logic diagram. This block allows you to display only the output in the diagram.

Hybrid Activity

Contains state-based logic. You can define different logic for each state in the chosen enumeration set. You also can add the Hybrid Activity to the State Tables. For information on working with this block, see Configuring a Hybrid Activity in the Configuring a System section.