Line Segment - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Line Segment logic block provides linear scaling and biasing of an input value using one or more line segments where two points define a single line segment.

The Line Segment block reliability values are Reliable or Math Error. The Present Value retains its previous value on Math Error. The block remains reliable if the input is not reliable (ignores unreliability of the input).

You must open the Details view of this block to configure its Input Points and Output Points. See Configuring the Line Segment Block in the Configuring a System section.

The following table describes the inputs and outputs of the Line Segment logic block.

Table 1. Line Segment Block Inputs and Outputs

Name

Data Type

Exposed for Connection by Default

Description

Default Value

Inputs

Clamp First

Boolean

No

Indicates the behavior when the Input is less than the first value in the Input Points array.

True

Clamp Last

Boolean

No

Indicates the behavior when the Input is greater than the last value in the Input Points array.

True

Input

Float

Yes

Indicates the signal that is transferred to the Present Value based on the line segment that the input falls within.

0.0

Outputs

Present Value 1

Float

Yes

Indicates the result of the linear scaling and biasing performed by the block.

0.0

Properties

Input Points

Float Array

N/A

Provides an array of values that contains the X values for the break points of the linearization.

0, 100

Number of Segments plus 1

Output Points

Float Array

N/A

Provides an array of values that contains the Y values for the break points of the linearization.

0, 100

Number of Segments plus 1

1 This input or output is the Default Element of the block.