Activity Outputs - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Activity Outputs folder in the control block palette contains Boolean, float, and enumeration output blocks. Use Activity Outputs to provide an outgoing connection point to custom logic modules.

Note: The tool automatically creates and configures the hierarchy table in a translation block when you connect an Activity Input block to an Activity Output block of a different type (Boolean to two-state Enum or two-state Enum to Boolean).
Table 1. Activity Output Blocks

Type

Description

Output (Boolean)

Provides a Boolean output for connections from other blocks in the logic diagram (True or False).

Output (Enum)

Provides an enumeration (Enum) output for connection from other blocks in the logic diagram.

Output (Float)

Provides a floating (Float) output for connection from other blocks in the logic diagram (numeric value).