Activity Inputs - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Activity Inputs folder in the control block palette contains Boolean, float, and enumeration input blocks. Use Activity Inputs to provide an incoming connection point to custom logic modules.

Note: The tool automatically creates and configures the hierarchy table in a translation block when you connect an Activity Input block to an Activity Output block of a different type (Boolean to two-state Enum or two-state Enum to Boolean).
Table 1. Activity Input Blocks

Type

Description

Input (Boolean)

Provides a Boolean input for connection to other blocks in the logic diagram (True or False).

Input (Enum)

Provides an enumeration (Enum) input for connection to other blocks in the logic diagram.

Input (Float)

Provides a floating (Float) input for connection to other blocks in the logic diagram (numeric value).