Object Attributes - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Each object section in the Help contains a table describing the object’s attributes. The columns in the object attribute tables provide the following information:

  • Name: Indicates the name of the attribute/parameter.

  • Type: Indicates the attribute/parameter type. Options include:
    • All Types: Indicates if the attribute/parameter appears in all types: Input, Output, Network Input, Network Output, Miscellaneous Input, and Miscellaneous Output.

    • Input: Indicates if the attribute/parameter appears for an Input or Miscellaneous Input module.

    • Network Input: Indicates if the attribute/parameter appears for a Network Input module.

    • Network Output: Indicates if the attribute/parameter appears for a Network Output module.

    • Output: Indicates if the attribute/parameter appears for an Output or Miscellaneous Output module.

  • Mode: Indicates the view mode of the attribute/parameter. Options include:
    • All Modes: Indicates if the attribute/parameter appears in all modes: Configuration, Simulation, and Commissioning mode.

    • Simulation: Indicates if the attribute/parameter appears in the Simulation mode.

    • Commissioning: Indicates if the attribute/parameter appears in the Commissioning mode.

    • Network Input and Network Output Configuration Mode Only: Indicates if the attribute/parameter is for Configuration mode only (for Network Input and Network Output modules).

  • Description: Describes the function of the attribute/parameter. Along with the descriptions, the attributes/parameters can be defined as:
    • Default Element (Generated State, if applicable): Identifies the attribute/parameter designated as the logic’s Default Element, which appears in the Control View columns below the module name. If applicable, the attribute/parameter is also a state generated by the module’s logic.

    • Visible in an Analog Input SAB Device: Indicates if the attribute/parameter appears for an Analog Input device on the SA Bus.

    • Calculated Value (Outputs): Indicates if the attribute/parameter is a value calculated by object’s logic and configuration in the State Tables. This attribute/parameter appears in the Parameters table in the Control View and/or in the Details dialog box.