Economizer Suitability (HP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
When selected, the Economizer Suitability options create Proportional Damper Output Controller, Mixed Air Damper Output, and Minimum Position Determination Logic. The Economizer Availability Determination Setpoint module is also created and interfaced to the Economizer Suitability option selected.

The selection options for Economizer Suitability are:

  • Network Command

  • Binary Input (Enthalpy Switch)

  • Outdoor Air

    • Dry Bulb Temp Economizer

    • Temp & Enthalpy Economizer