The following information is new for release 13.1:
- Added support for Series Network Controllers (SNCs) in Controllers Supported and documented SNC Controller SNC BACnet and Controller OID Limits in System Capacity Indicator. For additional information on SNC controllers, refer to the SNC Commissioning Guide (LIT-12013295).
- Added information about the new Save a Copy option in Table 1. Use this feature to save a copy of a CAF without modifying the working copy.
- Documented the options available when you launch CCT using the System Configuration Tool (SCT) in Table 1 and in Transfer to Device Wizard.
- Added information about a new feature available at Release 10.4 / Firmware 8.0 in Release Mode 10.4 / Firmware 8.0 and Later.