All applications require a zone temperature sensor. This input defaults to a SAB signal to use a network sensor and not consume additional IO points. The Setpoint Adjust option allows you to choose either Common Setpoint Adjust or a Warm Cool Adjust. You may also optionally select to add Temp Occ Support to include an input for temporary occupancy requests. The Fan Speed Adjust option adds a interface for specific Network Sensor models.