Discharge Air Temperature (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option is used primarily as a commissioning check-out feature to verify that the Discharge Air Temperature responds to commands to the heating and/or cooling devices.