Modulated (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option allows you to select the type of actuator.
  • Proportional: Select this option if the coil is controlled by a proportional valve that takes a 0–10 VDC or 4–20 mA signal.

  • Incremental: Select this option if the coil is controlled by an incremental valve that uses two binary outputs to incrementally open and close the valve.

  • Two Position: Select this option if the coil is controlled by a two position valve that uses a binary output to open and close the valve.