ModifyDevice Dialog Box - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See the Modifying Points on an SA Bus Device section.

Table 1. Modify Points Dialog Box

Field

Description

Add

Use to select whether or not to add the point to the device.

Type

Point type.

Function

Point function.

Data Type

Point data type.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.