See the Defining Hardware section.
The Add Devices dialog box appears after you select an I/O Module device to add in the SA Bus Device Selection dialog box. Use this dialog box to name your device.
Field |
Description |
---|---|
Device Name |
Device name. |
Quantity |
Use to select the number of I/O modules (see Set Maximum Quantity Dialog Box). |
Starting Index |
Use to enter the starting index for the I/O Modules you are adding to your system. |
OK |
Applies the changes and closes the dialog box. |
Cancel |
Closes the dialog box without applying the changes. |
|
Opens the Help system. |
|
Opens the Set Maximum Quantity Dialog Box. |