Modifying Points on an SA Bus Device - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
About this task

You can only add points to an SA Bus device if the device is a Network Sensor (Network Duct Sensor, Network Zone Sensor, or Network CO2 Sensor), Wireless Refrigerator/Freezer Temperature Transmitter and Probe Assembly (Network Cooler/Freezer Sensor), Wireless Sensor (Network Zone Sensor), or a Network VSD.

To add points to an SA bus device:

Procedure

  1. In the SA Bus Devices section of the Controller Selection tab, select the device you want to add points to.
  2. Click Modify Device. The Define Sensor dialog box appears.
  3. Select the check boxes next to the points you want and click OK. The tool adds the points to the device.
    Note: Highlighted points in the software indicate standard points that are coupled with the selected device type. The standard point selections are guidelines and are not required to be present on a device.