Importing Package Files - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
About this task

Use the Import feature to import packages.

Procedure

  1. Click Define Hardware.
  2. On the Packages tab, click Import, and then navigate to the package file that you want.
    Note: Field controller packages show the status Licensed or Unlicensed in the Packages tab. If a field controller package is unlicensed, the CAF can be opened as pseudo-artificial.
  3. Click OK.