Defining Hardware - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
You can define hardware by using the Define Hardware dialog box. You can complete the following tasks:
  • define the hardware, map points, and define network settings for the system.
  • review the device packages that are installed in the tool.
  • define the default devices for each system type.
  • create, remove, modify, and view application point mapping for a Serial N2 Slave object in a controller.