Current Output (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for Current Output are:

  • Current Output (AO): This option adds analog outputs with a signal of 4-20 mA for up to six devices.

    • 1 Output (AO)

    • 2 Outputs (2 AOs)

    • 3 Outputs (3 AOs)

    • 4 Outputs (4 AOs)

    • 5 Outputs (5 AOs)

    • 6 Outputs (6 AOs)