Command Motor (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection options for Command Motor are:

  • Command Motor (BO): This option indicates the command to the motor.

    • Status (BI): This option indicates whether the motor is running based on the motor command for up to six motors.

    • Quantity

      • One

      • Two

      • Three

      • Four

      • Five

      • Six