The Command Heat Tape selections load the following modules in this Control View column:
Outputs
-
HTAPEX-C (Heat Tape X Command BO, where X is 1-6): This Output is loaded when the Command Heat Tape (BO) node is selected. Specific Outputs are loaded per sensor.
See the Output Modules section.