Command Heat Tape (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection options for Command Heat Tape are:

  • Command Heat Tape (BO): This option is used to command heat tape to warm piping under freeze conditions for up to six locations.

    • 1 Output (BO)

    • 2 Outputs (2 BOs)

    • 3 Outputs (3 BOs)

    • 4 Outputs (4 BOs)

    • 5 Outputs (5 BOs)

    • 6 Outputs (6 BOs)