Display Configuration - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
You can customize what information displays in the MAP Gateway UI or on the DIS1710 controller display.

For MAP Gateway, the Display widget allows you to:

  • define which folders and points appear on the home page

  • define the order and groupings of folders and points on the home page
  • edit point user names and descriptions using the Mass Edit feature

After you configure the display, transfer the application to the controller, and then click Rediscover Devices in the MAP Device List page. The MAP Gateway is alerted and reads the new display information.

For DIS1710, the Display widget allows you to:

  • define which folders and points appear on the display panel (Idle, Inputs and Outputs, Parameters, and one User Defined pages that you see in the display)

  • define the order and groupings of display panel folders and points
  • auto populate folders for DIS1710 configuration
  • define which points are read-only (cannot be commanded using the display)

  • edit point user names and descriptions using the Mass Edit feature

  • set display attributes including contrast and backlight intensity

  • select timeout settings

  • select authorization including password definition

After you configure the display, transfer the application to the controller. The changes then become effective.