Using the Launch Wizard - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. Drag the Launch Wizard from the control block palette to the logic diagram in the right panel. The New Module Selection dialog box appears. See the New Module Selection screen section.
  2. Type the name of the block to locate in the Filter field. The search displays and filters results for each letter you type regardless of where the letter appears in the block name. For example, if you type co, Constant appears as well as ACOS and Lead Compensator. Your filter text is indicated by the bolded letters of the block name. You can click the Name column heading to sort the results in alphabetical or reverse alphabetical order.
    Note: The filter box is not case-sensitive.
  3. Click the Count box next to the block you want to add and adjust the number of blocks to add using the up and down arrows. Green highlighting appears when you change the quantity. To add another block, go back to Step 2 and search for that block name. You do not need to close the Launch Wizard to add a different block.
  4. When you have finished adding blocks, click Finish. The blocks you added appear in the logic diagram.