Duplicating a Block - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The duplicate feature copies and pastes the selected blocks, including any connections, in one step. When you duplicate a block, you can only paste into the same state section or activity of the blocks that you duplicate.

To duplicate a block in the Logic View:

Right-click the block and select Duplicate. To duplicate multiple blocks at once, press and hold the Ctrl key while selecting each item, and then select Duplicate. When you duplicate multiple blocks, the block connections are also duplicated.

Note: You also can select a block and use the Ctrl-D keys to perform this function.