Deleting a Connection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

About this task

See the Logic Tab Screen description in the User Interface section.

To delete a connection line:

Procedure

  1. Right-click the connection line or hidden edge label (numbered circle next to an Activity Input, Activity Output, block input, or block output: , , or ) and select Delete. The Confirm dialog box appears asking you to confirm the deletion. See the Confirm (Delete) screen section.
    Note: You also can select a connection line or hidden edge label and press the Delete key to perform this function.
  2. Click Yes.
    Note: When a hidden edge label indicates multiple connections (for example, 1:5), only the connection added last is deleted. If you need to delete a specific connection, unhide the connection lines and remove the appropriate connection.