Adding a Column to the State Selection Tables - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. Click the State Tables tab. The State Tables tab appears with the system’s state selection data populated within tables in the right pane, and the states in the left pane of the tab. The panes allow you to scroll both vertically and horizontally, keeping the first column visible. See the State Selection (State Tables Tab) screen section.
  2. Click Edit.
  3. Right-click the module name (table heading: yellow = connected or orange = not connected) and select Create State Selection Column. The Create State Selection Column dialog box appears.
  4. Type a name in the Name field.
    Note: We recommend leaving this field empty so that dynamic naming may be used.
  5. Select where you want the column to appear in the table using the Column Index drop-down menu.
    Note: Selecting 1 places the column in the leftmost column position.
  6. Select the type of data for the column (Enumeration or Boolean).
  7. Click OK.
  8. Click Apply.