System Selection Wizard - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Selecting a System (Creating a New System) and Viewing and Modifying System Selections.

Table 1. System Selection Wizard

Field 1

Description

Mechanical System Selection Screen

Select the mechanical components to use in your system by browsing through the folders of the selection tree and selecting the check boxes and radio buttons. For information on the types of systems you can create and details on the selections available, see the User Interface and Applications sections.

Control Logic Selection Screen

Select the control logic to use in your system by browsing through the folders of the selection tree and selecting the check boxes and radio buttons. For information on the types of systems you can create and details on the selections available, see the User Interface and Applications sections.

Previous

Moves to the previous screen of the wizard.

Next

Moves to the next screen of the wizard.

Finish

Applies the selections and closes the wizard. The system appears in the Control View in Configuration mode.

Cancel

Closes the wizard without applying the selections.

Opens the Help system.

System Selection Module Help (F1)

Opens the module Help. As you make selections in the System Selection Wizard, you can press F1 to view the Help screen. The Help screen displays the module Help section for the item you are viewing and changes as you select different items in the wizard. Click the links on the Help screen to view module information.

1 For Sideloops, there is only one Selection screen called Sideloop Selection. The Previous button is enabled but does not work. The Next button is disabled. For information on creating sideloops, see the Creating a Sideloop section.