Mode Selection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Configuring the MUX Block.

Table 1. Mode Selection

Field

Description

Mode

Use to select a value to use for the input mode of a MUX block.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.