Some items in the lists may appear disabled because they are automatically exposed for connection and cannot be changed, or if they are already connected. See Exposing Ports for Connection and Exposing Ports.
Field |
Description |
---|---|
Filter | Provides text box to search the selection tree based on the node name. The search results include the matching node and its ancestors. |
Input Port List |
Lists the input ports you can hide or expose for connections and allows you to select ports using check boxes. |
Output Port List |
Lists the output ports you can hide or expose for connections and allows you to select ports using check boxes. |
Select All |
Selects all input/output ports in the Input Port List and Output Port List. |
Deselect All |
Removes the selection of all input/output ports in the Input Port List and Output Port List. |
OK |
Applies the changes and closes the dialog box. |
Cancel |
Closes the dialog box without applying the changes. |
|
Opens the Help system. |