The Clone Ports dialog allows you to duplicate ports of a block. Only ports that are exposed and not connected can be duplicated; you cannot duplicate ports that are both exposed and connected. See the Cloning a Port section.
Field |
Description |
---|---|
Input Port List |
Lists the input ports you can duplicate. |
Output Port List |
Lists the output ports you can duplicate. |
Select All |
Selects the check boxes of all input/output ports in the Input Port List and Output Port List. |
Deselect All |
Clears the check boxes of all input/output ports in the Input Port List and Output Port List. |
OK |
Applies the changes and closes the dialog box. |
Cancel |
Closes the dialog box without applying the changes. |
|
Opens the Help system. |