Adding an Exception Schedule - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
About this task

You can add exception days to your schedule. Exception days can be holidays or a range of days with modified hours (for example, summer hours).

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, right-click Schedules and click Add Schedule. A new schedule is added to the Advanced Object tree.
  4. Click the schedule located below Schedules in the Advanced Object tree.
  5. Click Edit. The fields you can edit appear in white.
  6. Enter the basic parameters. See Adding a Basic Calendar.
  7. In the Display Mode list, click Exception Schedule.
  8. Click the + button. The Exception Detail screen appears. See Exception Detail Screen.
  9. Define the parameters of the exception schedule.
  10. Click OK.
  11. Click Apply.