Schedule Details Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Schedule Screen

Field

Description

Object - Name

Indicates the name of the schedule.

Description

Indicates the description of the schedule.

Enabled

Indicates if the schedule is enabled (True) or disabled (False).

Object Identifier

Indicates the read-only ID of the schedule.

BACnet - Priority for Writing

Indicates the priority of the schedule. The lower the number, the higher the priority.

Operation and Display - Effective Period

Indicates the time frame that the schedule is in effect. Click the browse button to define this information.

Schedule Output Type

Indicates the output type of the schedules: Binary, Analog, and Multistate.

Default Schedule Command

Indicates the default text that appears when you create the schedule: Release (Binary, Analog, Multistate), Off, or On.

Note: If the Default Schedule Command is set to Release, the scheduling feature’s control over the scheduled items ends. Release should only be used for the Default Schedule Command if the scheduled items support the Release command.

States Text

Indicates the state text options used when you view and create the schedule.

Display Mode

Indicates the available schedule display modes: Weekly Schedule, Exception Schedule, and Exception Items.