Exception Detail Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Exception Detail Screen

Field

Description

Date

Use to add a custom date to the calendar.

Date Range

Use to add a date range to the calendar.

Week and Day

Use to add an e Annotation element to the other elements inclusion list If docType.hasElementType("Annotation") And docType.hasElementType("Article") Then docType.addElementToInclusions "Annotation", "Article" End If End If End If End Function doaddElements() m rootElem rootElem = docType.name ' Application.Alert rootElem If rootElem = "Article" And Not docType.hasElementType("Annotation") Then ' add Annotation element docType.addElement "Annotation", "Annotation" , True , False ' check if element is added (it won't for schemas) If docType.hasElementType("Annotation") Then ' add attribute UserName docType.addAttribute "Annotation", "UserName", "", 0, 0