Recipients Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Editing Device Information.

Table 1. Recipients Screen

Field

Description

Recipients

List of recipients.

Add

Use to add a recipient. See Notification Recipient Screen.

Remove

Removes the recipient from the list.

Moves the selected recipient up in the list of recipients.

Moves the selected recipient down in the list of recipients.

Details

Opens the Notification Recipient dialog box, which displays details of the recipient. See Notification Recipient Screen.

Save

Saves changes to the information in the screen.

Cancel

Exits the screen without saving changes

Opens the help system.