Notification Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
See Setting up Device Notification.

Table 1. Notification Screen

Field

Description

Object Name

Indicates the name of the notification.

Description

Indicates the description of the notification.

Enabled

Indicates if the notification is enabled (True) or disabled (False).

Object Identifier

Indicates the read-only BACnet object identifier for the notification.

BACnet - Ack Required

Indicates To Off Normal, To Fault, and To Normal events, respectively.

Priority

Indicates the priority to be used for event notifications for To Off Normal, To Fault, and To Normal events, respectively. A lower number indicates a higher priority.

Recipient List

Indicates the list of one or more devices which notifications are sent. For more information, see Notification Recipient Screen.

Send Notification to Supervisor

Indicates if you want to send the notification to a supervisory controller.

Supervisory Device Process ID

Indicates the process ID of the supervisory controller that receives the event notification messages.