Restoring Flow - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. In the details view of the Balancer Override SD module, click Flow Restore. The Flow Restore Command dialog box appears asking if you want to send the restore flow command.
  2. Click Send.

    Return to the Using the Balancing Feature section.