Procedure
- In the details view of the Balancer Override SD module, click Flow Override. The Flow Override Command dialog box appears.
- Select a value from the menu. For example, select Supply Duct Max to drive the VAV Box Controller to the maximum cfm.
-
Click Send to issue the command.
Return to the Using the Balancing Feature section.