Editing the Balancing Attributes - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. Right-click the Balancer Override SD module and click View Details.
  2. Click Edit.
  3. Modify the attributes as desired (for example, change the flow setpoints).
    Note: Click Cancel to exit Edit mode without applying changes.
  4. Click Apply. The changes are made and the system exits Edit mode.

    Return to the Using the Balancing Feature section.