Autocalibrating the VAV Box Controller - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  1. Right-click the Balancer Override SD module and click View Details.
  2. Click Auto Calibrate. The Auto Calibrate Command dialog box appears asking if you want to autocalibrate the device.
  3. Click Send.

  4. Monitor the Autocal Status attribute in the Status section of the attribute table:

    • When False, the autocalibration is in progress and the task buttons are inactive.

    • When True, the autocalibration is complete and the task buttons are active.

Note: Autocalibration takes approximately 60 seconds to complete, which is the stroke time of the actuator over 90 degrees of travel.

Return to the Using the Balancing Feature section.