Using the Balancing Feature - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Note: The task buttons of the balancing feature are active only when in the Test mode; however, you do not need to be in Test mode to edit the attributes of the Balancer Override module.

The following steps describe a typical use of the balancing feature:

  1. Start the Test mode. See Starting the Test Mode.

  2. Edit the VAV Box Controller balancing attributes such as Flow Setpoints to the desired values, if necessary. See Editing the Balancing Attributes.

  3. Autocalibrate the VAV Box Controller. See Autocalibrating the VAV Box Controller.

  4. Issue a Flow Override command to measure the flow in the space (for example, drive the VAV Box Controller to the maximum cfm). See Issuing a Flow Override Command.

  5. Exit the Test mode. See Stopping the Test Mode.