Making an NxE Passthru Connection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
To make an NxE Passthru connection from this tool to the Metasys NAE, on the Transfer screen, enter the device host name or IP address (or select the device host name or IP address from the drop-down menu), enter your user credentials, and click Login.

Notes:
  • You do not need to launch the tool or have a supervisory device configuration tool to use the NxE Passthru connection. When the tool is launched from the supervisory device configuration tool, the supervisory device connection information is not automatically populated.
  • If you have selected Current Application, only the Field Device defined in your CAF appears in the selection list.