Viewing Online Operations - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
You can view controller information for a single controller in Commissioning mode. This option is not available in the Simulation mode. Use this procedure to access information from the controller to which you are connected and commissioning. You can open a CAF to view controller information, or select a connection type and discover controllers to view multiple controller information.

To view the details of the controller being commissioned, click Online Operations on the Tools menu.

Note: For information on viewing controller information from the Configuration mode, see the Configuring a System section.