Showing and Hiding Involvement - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
About this task

You can view involvement in two ways—within the UI or through a Show Involvement dialog box.

If you want to view involvement in a separate dialog box, first click Settings, then select Use Involvement Dialog.

Procedure

  1. Right-click an output and select Show Involvement. If you selected the Use Involvement Dialog setting, the Show Involvement dialog box appears.

    The magenta background color change indicates which modules are affecting the selected output. See Control Tab Status Colors and Icons in the User Interface section for more information.

  2. To hide involvement, right-click an output and select Hide Involvement. If you selected the Use Involvement Dialog setting, click Close.