Modifying the Polarity of Position Adjust Outputs (PAOs) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. Right-click an output or miscellaneous output and select View Details. The Details dialog box appears.
  2. Click Edit.
    Note: When in Edit mode, the system stops polling data until the window closes. System data polling immediately resumes when the dialog box is closed.
  3. Enter the desired PAO value.
  4. Click OK.