Table 1 describes the screens in the Commissioning Device Wizard. See the Commissioning a Device section.
Field |
Description |
---|---|
Transfer Type |
Use to select either the current Controller Application File (Current Application) or a Controller Application File in the device (Application in Controller). When you select Application In Controller, the wizard transfers the file from the device to the computer. Note: To commission a device that contains an existing application, use the Applications in Controller setting to make sure you commission the latest information.
|
Connection Type |
Use to select an NxE Passthru, Bluetooth, MAP 4.2+/BACnet Router, Direct Ethernet, ZigBee, or Direct Ethernet Connection. |
Connection Parameters |
|
Discovery |
Use to perform Auto, MAC Address, or Instance Number based Discovery depending on your connection type. |
Field |
Description |
---|---|
Device Name |
Device name after the discovery process finishes. |
System Name |
System name after the discovery process finishes. |
Address |
Controller’s address after the discovery process finishes. |
Type |
Type after the discovery process finishes. |
Status |
Status after the discovery process finishes. |
Instance Number (BACnet ID) |
BACnet® ID. Note: If more than one device has the same Instance Number, the numbers display red in the device list.
|
Previous |
Moves to the previous screen of the wizard. |
Next |
Moves to the next screen of the wizard. Note: This option is disabled if a device with a duplicate Instance Number is selected.
|
Cancel |
Closes the wizard without starting Commissioning mode. |
|
Opens the tool Help system. |
Field |
Description |
---|---|
Device Information |
Displays information for the following:
|
Status |
Status of entering Commissioning mode after clicking the Finish button. |
Previous |
Moves to the previous screen of the wizard. |
Finish |
Closes the wizard and starts Commissioning mode. |
Cancel |
Closes the wizard without starting Commissioning mode. |
|
Opens the Help system. |