Test Mode - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Test mode allows you to see the effects of commanding inputs, modules, and outputs to assist in commissioning your system. During Test mode, the controller being commissioned is taken offline from the supervisory system. Any commands you make update the values within the user interface, but the actual hardware values do not change. You must exit Test mode before you exit the Commissioning mode. See the Working with the Test Mode section.