Commissioning a System - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Tool commissioning option lets you commission your device with or without a CAF. In the Commissioning mode, you can make NxE Passthru or Wireless connections, work with the Test mode, and balance VAV Box Controllers.

Note: If you are running the Commissioning software, this section describes the main tasks available to you. The Commissioning topic in the User Interface section describes this software version.
When viewing live data in the Commissioning mode, changing values are highlighted in various colors. The color of the highlighting is determined by the frequency that the value changes. As poll cycles return consistent values, the highlighting fades away. The intention of this feature is to bring to attention changes across the application's data system, expose potential relationships between values and modules, and assist in troubleshooting.
Notes:
  • Temporary color highlighting appears in three color stages (blue, yellow, and red). After the third stage (red), all subsequent consecutive changes continue to display red. For more information on status color, see Table 1.
  • The parameter change color highlighting feature can be turned on or off from the Commissioning mode's control bar.