Heating Options (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection options for Heating Options are:

  • Boiler Status: This option monitors the boiler status.

  • Boiler General Alarm: This option monitors the general alarm status of the boiler.

  • Boiler High Temp Alarm: This option monitors the high temperature alarm status of the boiler.

  • Boiler Flow Switch: This option monitors the flow switch status of the boiler.

  • Combustion Air Damper: This option controls a combustion air damper for the boilers.

    • End Switch: This option monitors the combustion air damper status.

  • Primary Hot Water Supply Temp: This option monitors the leaving or primary supply water temperature of each boiler.

  • Primary Hot Water Return Temp: This option monitors the entering or primary return water temperature of each boiler.

  • Primary HW Flow Sensor: This option measures the primary hot water flow.

  • Main Steam Header Pressure: This option monitors the main stream header pressure.